Technical FAQs

Ask a Question

What is the replacement for the VW3A21315 Bacnet card?

Issue:
Customer is looking for the replacement for obsolete VW3A21315, Bacnet option card.

Product line:
ATV21, SFD21

Environment:
all

Cause:
Obsolete

Resolution:
The VW3A21315 is an optional Bacnet communication card for the obsolete ATV21 drives.  The newer ATV212 drives come with Bacnet built into the device.  There is no replacement for the card alone.  
 
Was this helpful?
What can we do to improve the information ?