Technical FAQs

Ask a Question

Osisense XC - How to order XCKM1 limit switch reference

XCKM1 part number is not the reference of a complete limit switch. It is either the ZCKM1 contact body, either an incomplete commercial reference. Please check the head reference and the possible arm reference to pass order. It could be an obsolete XCKM1* limit switch like shown on the attached picture. In this case, please refer to the attachment giving a cross-reference table.

Was this helpful?
What can we do to improve the information ?