Technical FAQs

Ask a Question

Video: How to Determine ION86xx Series MAC Address

Issue
The procedure to determine an ION86xx series MAC address.

Product Line
PowerLogic ION8600 series (A/B/C), ION8650 series (A/B/C)

Environment
Front Panel Display

Cause
Some customers require the MAC address of an ION86xx series meter as part of their network setup.

Resolution
The steps to determine the MAC address are as follows:

1. Press and hold Alt / Enter to get to setup mode
2. Press and release down arrow key a few times to get to Network Setup, press Alt / Enter
3. Press and release down arrow key a few times to get to MAC Address, press Alt / Enter
    MAC address will be displayed
4. To exit setup mode, press Alt / Enter key a few times.

This video demonstrates this procedure:

Was this helpful?
What can we do to improve the information ?