Browse FAQs

Osisense XC - How to order the XCKJ50543C limit switch outside China

Published date: 01 March 2019

The XCKJ50543C limit switch (or ZCKJ5C body + ZCKE05C + ZCKY43C) is an XCKJ limit switch produced in China for their market. It cannot be ordered outside China through our international distribution centers. To replace such reference outside China, you have to order the XCKJ reference without C at the end. in this case, XCKJ50543 limit switch to be order under the following sub-assemblies ZCKJ5 body having a Pg 13.5 cable entry (or ZCKJ5H29 ...) + ZCKE05 head + ZCKY43 variable length steel roller lever.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.