Technical FAQs

Ask a Question

What is the voltage level on which the iC60N circuit breakers can be used in DC circuit?

The iC60N circuit breakers are compliant with maximum 60V DC / pole for a breaking capacity of 15kA.
1P iC60N -> up to 60V DC
2P iC60N -> up to 125V DC
3P iC60N -> up to 180V DC
4P iC60N -> up to 250V DC

The iC60N circuit breakers are compliant with maximum 72V DC / pole for a breaking capacity of 10kA.
1P iC60N -> up to 72V DC
2P iC60N -> up to 144V DC
3P iC60N -> up to 216V DC
4P iC60N -> up to 288V DC
Was this helpful?
What can we do to improve the information ?