Browse FAQs

Preventa XU - XUSL safety curtains - CSA certificate

Published date: 16 May 2019

The safety light curtains XUSL4E* type 4, the XUSL2E* type 2 and the safety light curtains with integrated muting fonction XUSL4MA* & XUSL4MB*, are not CSA marked. They are cULus listed by the UL, and this mark appears in the transmitter and the receiver. If a product is cULus listed, it means that UL tested the product to meet all the requirements under Canadian and US standards. Anything that has cULus mark can be used both in Canada and US. Find attached corresponding certificate NIPF7.E198201 for the XUSLN, XUSLP, XUSLB/DM, XUSL2E/4E and XUSL4MA/MB safety light curtains (AOPD)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.