Technical FAQs

Ask a Question

How to simulate motor loads in Ecodial Plugin for AutoCAD?

While editing the load properties, in the field Motor Load select "Yes". Now you can observe that the symbol changes from Passive load to Motor loads. After the calculation, you can see the contribution of motor loads increasing the short circuit current.
Was this helpful?
What can we do to improve the information ?