Technical FAQs

Ask a Question

What is the purpose of the D_ON_X on the Unity Pro PID1 function block

When the D_ON_X is FALSE the Derivative contribution is coming from TD.  
When D_ON_X is TRUE, the Derivative contribution comes from the Process Variable.

 
 
 
Was this helpful?
What can we do to improve the information ?