Technical FAQs

Ask a Question

Ethernet connected Onicon meter is not communicating in Power Monitoring Expert

A translator file is created for Onicon flow meter in PME.  An Ethernet device is created in PME with an IP address, however, the device does not communicate.

Product Line
Onicon Flow Meter

Modbus Device Importer (MDI)
Management Console

A Modbus address is associated with the Onicon device.

Onicon flow meters have a default Modbus address of 17.  This address should be included in 'Unit ID' of the Ethernet device in Management Console.

1. In Management Console, open the property of the Ethernet device
2. Right click and select 'Advanced Properties'
3. Set the address in 'Unit ID' field

NOTE: If the Modbus address is not set, it reverts to default of 255.

Onicon Modbus manual (D-100 Modbus) can be downloaded from Onicon website.
Was this helpful?
What can we do to improve the information ?