Technical FAQs

Ask a Question

In the NSX Micrologic 5 and 6 trip units, for which trip events is the interrupted current stored in the trip record log file?

For electrical distribution application, the interrupted current is measured and stored when a trip occurs, due to:
1. long-time protection;
2. short-time protection;
3. instantaneous protection.

For motor-feeder application, the interrupted current is measured and stored when a trip occurs, due to:
1. short-time protection.

In case of other trip types, the interrupted current is not measured and stored.
Was this helpful?
What can we do to improve the information ?