Technical FAQs

Ask a Question

How to read the RTU time from SCADAPACK RTU using E configurator?

The Get RTU Time command returns the local or UTC (Coordinated Universal Time) time in the selected SCADAPack E RTU.

To read the RTU time

1.Select Transfer > Get RTU Time. The Read RTU Time dialog appears.


2.Select one of the following:

·Use UTC time: Select Use UTC time to read the RTU time in UTC (Coordinated Universal Time) time.

·Use local (PC) time: Select Use local (PC) time to read the RTU time in the time set on the PC.

3.Click OK. The following status window is displayed:

4.Click OK to close the dialog and return to the main window.

Was this helpful?
What can we do to improve the information ?