Technical FAQs

Ask a Question

What is the braking resistor minimum value for an ATV71HC20Y?

Issue:
Looking for the braking resistor minimum ohmic value for an ATV71HC20Y

Environment:
Altivar 71

Product Line:
Variable Frequency Drives

Cause:
Need to know what is the minimum ohmic value the drive can accept as a braking resistor

Resolution:
The minimum ohmic value of the braking resistor is 2ohms
You need to use the braking unit VW3A7103 as it is not included inside the drive.


 
Was this helpful?
What can we do to improve the information ?