Technical FAQs

Ask a Question

What is the braking resistor minimum value for an ATV71HC20Y?

Issue:
Looking for the braking resistor value for an ATV71HC20Y

Environment:
Altivar 71

Product Line:
Variable Frequency Drives

Cause:
Need to know what is the minimum value the drive can accept as a braking resistor

Resolution:
The minimum value of the braking resistor is 2ohms
You need to use a braking unit, part number VW3A7103.  This is not included with the drive by default.


 
Was this helpful?
What can we do to improve the information ?