Yes, it is possible to set date and time of TESYS T in SoMove:
- LTMR has to be connected to SoMove
- in SoMove click on: Device - Maintenance - Set Device Date Time (see Attachment1)
- the date and time will be updated automatically from PC (it will be the same like PC date and time)
Please notice that if power of LTMR is turned Off for more than 30 minutes, the LTM R controller resets its internal clock to the time when power was turned Off.
The Date and Time is stored in registers 655 to 658, the format is described in Attachment2.