Browse FAQs

Preventa XCS - XCSLF3535612 wiring diagram

Published date: 10 June 2019

Find attached the wiring diagram of the XCSLF3535612 safety switch, having 1NC + 2NO main contacts, and 1NC + 2NO electromagnet contacts. It is a version with locking by electromagnet on de-energisation and an escape release button in the enclosure rear. The electromagnet contacts are represented electromagnet not energised. Such diagram is supplied inside the switch.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.