Technical FAQs

Ask a Question

Application Services Host does not Connect to Citect Data Platform

In Application Configuration utility > Application Services Host > Citect Data Platform, the user tries to test Citect credentials, but gets the following error even when Runtime is running:

                Citect connection unavailable.
                Note: Citect runtime must be running to perform this test.

Product Line
PowerSCADA Expert 8.2 (PSE 8.2)

Application Configuration Utility

CtAPI is unavailable

Adding the following parameter to Citect.ini file resolved the problem:
[CtAPI] Remote=1
Was this helpful?
What can we do to improve the information ?