Technical FAQs

Ask a Question

Using Performance Monitor (PerfMon) to Monitor SCADA Systems

Issue
Detailed examples of Performance Monitor data collector sets useful to troubleshoot SCADA performance issues.

Product Line
PowerLogic Scada 7.2
While this paper is based on PLS 7.2, it is general and can be used with other versions, including PowerSCADA Expert (PSE).

Environment
Performance Monitor (perfmon)

Cause
Performance Monitor is very useful for tracking and logging statistical data such as Memory/CPU usage as well as Citect performance counters.  This technical paper explains on how to use Windows Performance Monitor to monitor the Health/Performance of SCADA systems.
 
Resolution
Refer to attached technical paper for detailed instructions.
Was this helpful?
What can we do to improve the information ?