Technical FAQs

Ask a Question

Preventa XCS - XCSTE5312 wiring diagram

Find attached the wiring diagram of the XCSTE5312 safety switch, having 1NC + 1NO main contacts and 1NC electromagnet contact. It is a version with locking by electromagnet on de-energization. The electromagnet contact is represented electromagnet not energised. Such diagram is indicated on the front cover of the switch. The references XCSTE5311 & XCSTE5313 use it too.

Was this helpful?
What can we do to improve the information ?