Technical FAQs

Ask a Question

Preventa XCS - XCSTE7312 wiring diagram

Find attached the wiring diagram of the XCSTE7312 safety switch, having 2NC main contacts and 1NC electromagnet contact. It is a version with locking by electromagnet on de-energization. The electromagnet contact is represented electromagnet not energised. Such diagram is indicated on the front cover of the switch. The references XCSTE7311 & XCSTE7313 use it too.

Was this helpful?
What can we do to improve the information ?