Technical FAQs

Ask a Question

Preventa XCS - XCSE8512 wiring diagram

Find attached the wiring diagram of the XCSE8512 safety switch, having 3NC main contacts and 1NC + 1NO electromagnet contacts. It is a version with locking by electromagnet on energization. The electromagnet contacts are represented electromagnet not energised. Such diagram is indicated on the front cover of the switch. The references XCSE8511 & XCSE8513 use it too.

Was this helpful?
What can we do to improve the information ?