Technical FAQs

Ask a Question

Preventa XCS - XCSE83127 wiring diagram

Find attached the wiring diagram of the XCSE83127 safety switch, having 3NC main contacts and 2NC electromagnet contacts. It is a version with locking by electromagnet on de-energization. The electromagnet contacts are represented electromagnet not energised. Such diagram is indicated on the front cover of the switch. The reference XCSE83117 uses it too.

Was this helpful?
What can we do to improve the information ?