Technical FAQs

Ask a Question

Preventa XCS - XCSE73127 wiring diagram

Find attached the wiring diagram of the XCSE73127 safety switch, having 2NC + 1NO main contacts and 2NC electromagnet contacts. It is a version with locking by electromagnet on de-energization. The electromagnet contacts are represented electromagnet not energised. Such diagram is indicated on the front cover of the switch. The references XCSE73117 & XCSE73137 use it too.

Was this helpful?
What can we do to improve the information ?