Technical FAQs

Ask a Question

Preventa XCS - XCSE7512 wiring diagram

Find attached the wiring diagram of the XCSE7512 safety switch, having 2NC + 1NO main contacts and 1NC + 1NO electromagnet contacts. It is a version with locking by electromagnet on energization. The electromagnet contacts are represented electromagnet not energised. Such diagram is indicated on the front cover of the switch. The references XCSE7511 & XCSE7513 use it too.


Was this helpful?
What can we do to improve the information ?