Are the Acti9 and Multi9 contactor auxiliaries compatible with both Acti9 and Multi9 contactors?
The new and old generations of auxiliaries for contactors are equivalent and compatible for Acti9 and Multi9 contactor offers, except the iACT24 auxiliary.
The iACT24 is compatible only with the contactors of the Acti9 range.