Technical FAQs

Ask a Question

What is the depth of the NG125 device equipped with direct rotary handle?

The depth of the NG125 + direct rotary handle (reference number 19092 or 19097), measured from the back of the NG125 to the front point of the rotary handle is 100mm.
Was this helpful?
What can we do to improve the information ?