Technical FAQs

Ask a Question

What is the thread type and depth of the center bore found in the output shaft of GBX120032K gearbox ?

The center bore hole found in the output shaft of the GBX120032K gearbox is an M10 thread by 22mm deep.

See attached drawing.


rev 8-21-17
Was this helpful?
What can we do to improve the information ?