Technical FAQs

Ask a Question

How to set SCADAPACK RTU time using E configurator?

Set RTU Time is used to set the local or UTC (Coordinated Universal Time) time in the selected SCADAPack E RTU to the PC time.

To set the RTU time

1.Select Transfer > Set RTU Time. The Set RTU Time dialog appears.

2.Select one of the following:

·Use UTC time: Select Use UTC time to set the RTU to UTC (Coordinated Universal Time) time.

·Use local (PC) time: Select Use local (PC) time to set the RTU time to the time set on the PC.

3.Click OK to write the time to the RTU. The following status window is displayed:

4.Click OK to close the dialog and return to the main window.


Was this helpful?
What can we do to improve the information ?