Browse FAQs

M340 firmware encrypted?

Published date: 30 July 2019

The checksum is encrypted. 
It is only embedded in a built application (stu or sta), and not XML export format (zef or xef), so even more difficult to find it. 
M340/Unity has a cryptographic checksum. 
It is important to know that the software/firmware on an M340 Ethernet PLC is approved, tested and validated.
As such, each M340 PLC should have a known configuration of software and firmware.
The transit agency should be able to confirm that files on each PLC have not been tampered with.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.