Technical FAQs

Ask a Question

What is the tightening torque to be applied on the Canalis KSB tap off unit connection terminals?

Tap-off unit Screw size Tightening torque
KSB25SD4
KSB63SD4
fuse holder system installed in the tap-off unit 2.8Nm (Min 2.4Nm to 3.2 Max)
KSB160SE4/5
KSB160SF4/5
M8*16 15 Nm ( +- 20% )  (*)
KSB250SE4/5 Diameter of drill 13 mm choose in function of the screw (*)
KSB400SE4/5 Diameter of drill 11.8 mm choose in function of the screw (*)

(*) - Tightening torque values depending on the screw's nominal diameter are in the attached file.
Was this helpful?
What can we do to improve the information ?