Technical FAQs

Ask a Question

Is there an embedded timestamp object within ION protocol handles?

Issue
Further information with respect to how ION protocol handles timestamps is required. 

Product Line
PowerLogic ION meters

Environment
Intermediate/Advanced Metering

Cause
Requires an understanding of how the hisotircal data's timestamps are generated within the meter's onboard data log.
 
Resolution 

ION protocol does not have the capability to output the value (of the ION handle) and time-stamp simultaneously similar to DNP where each point has a ".timestamp" subtype object that stores the timestamp of the associated event. However, the meter can output this information via ION protocol through another method that outputs values and their respective timestamps. This is achieved over 2 separate requests, one for the value and the other for the timestamps. 

Refer to the following link for detailed instruction on using ION Test to read registers. 
FA219731

For example, to read the value of a register from an ION meter, it uses (Method 21 - Register_read_value)

· To read a register value from the meter, type:

0x<ion_handle> 21 void

· Replace <ion_handle> with a valid ION Handle in hexidecimal format In this example. 21 is the ION method number 21 which corresponds to ION_read_value and will return the value read from the specified ION register.

· If you get a value response from the device you will see the following:

  • 0x5800 21 void
    #Sent at: Mon Nov 01 15:23:20.173 2004
    #Recv at: Mon Nov 01 15:23:20.189 2004
    {
    119.812
    }
For example, to read the timestamp of the last change made to the ION module containing the register from an ION meter, it uses (Method 20 - Register_read_time)

· To read the timestamp of register from the meter, type:

0x<ion_handle> 20 void
· Replace <ion_handle> with a valid ION Handle in hexidecimal format.



The timestamp output from the meter will be in UNIX format which is a system for describing instants in time, defined as the number of seconds that have elapsed since 00:00:00 Coordinated Universal Time (UTC), Thursday, 1 January 1970, minus the number of leap seconds that have taken place since then. 

**ION meters that do not have a Clock Module within the framework (E.g. ION 7300 series) will not support the above. 

 
Was this helpful?
What can we do to improve the information ?