Technical FAQs

Ask a Question

How to inhibit the earth leakage protection function on a Masterpact circuit breaker equipped with Micrologic 7.0?

If the earth leakage protection of Micrologic 7.0* must be inhibited, the following steps must be followed:
1. Open the circuit breaker
2. Disconnect the rectangular sensor from the circuit breaker's terminal.
3. Link together the terminals M1+M2+M3 directly on the rectangular sensor. As current transformer technology, it is not recommended to leave the windings open.
                                                                           
      - link marked with blue.
4. In order to have a better protection against EMC disturbances, link together the terminals M1+M2+M3 on the terminal block of the circuit breaker.
                                                       
       - link marked with blue.
Was this helpful?
What can we do to improve the information ?