Technical FAQs

Ask a Question

Is it possible to control Lexium 28 via Modbus communication?

No, it is not possible to control LXM28 via Modbus.

Modbus control is not implemented into Lexium 28
It's possible to read and write parameters via Modbus, but it is not possible to control the drive via the Modbus channel because there are no
Modbus objects available on LXM28 for the "ControlWord" and also not available for the "ModesOfOperation"

Customers looking to control LXM28 via fieldbus need to select a PLC which supports CANopen.
Was this helpful?
What can we do to improve the information ?