Technical FAQs

Ask a Question

The 33193 resistor is compatible with Compact NS630b-1600 circuit breakers?

The 33193 additional resistor is compatible with the Compact NS 630b-1600 electrically operated devices equipped with a 380/415 V AC motor mechanism. The additional resistor must be connected if the supply voltage of the motor mechanism is 440/480V AC.

Connection schema:

A4 - electrical opening order;
A2 - electrical closing order;
B4, A1 - power supply for control devices and gear motor.
Was this helpful?
What can we do to improve the information ?