Browse FAQs

Does the M221 have the ability to load an application directly through FTP without SoMachine Basic V1.6?

Published date: 05 November 2018

M221 does not support FTP Server.
You must use SoMachine basic to load the application to the M221 remotely.
Or clone an application using an SD card.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.