Technical FAQs

Ask a Question

How may IEDs can be connected simultaneously with one MMS Client of the BMENOP0300 module?

We support up to 32 concurrent client connections (i.e. BMENOP0300 is client) to IEDs per module, you may add extra module(s) if you need more than 32 concurrent connections to IEDs.
Was this helpful?
What can we do to improve the information ?