Technical FAQs

Ask a Question

For MMS server of BMENOP0300, what logical nodes are supported?

You can configure MMS server data model with logical nodes defined in IEC 61850-7-4, IEC 61850-7-410 and IEC 61850-7-420 for substation automation, Hydro Power and Distributed Energy Resources.
Was this helpful?
What can we do to improve the information ?