Technical FAQs

Ask a Question

Why does Designer show 'ION' instead of the module icon for a PM8000?

Issue:
When opening a PM8000 in Designer on an ION Enterprise 6.0 system, certain modules show the word 'ION' rather than the appropreate icon shown in newer versions of PME. 

ION Enterprise 6.0 Designer Toolbox


Power Monitoring Expert 7.x Designer Toolbox


Product Line:
ION-Enterprise 6.0
Power Monitoring Expert 7.x / 8.x

Environment:
Designer toolbox icons

Cause:
ION Enterprise 6.0 does not contain the icons for the newer PM8000 modules. 

Resolution:
This issue is cosmetic and has no effect on meter programming or functionality. Hovering over the icon with the mouse will give the name of module type. 
Was this helpful?
What can we do to improve the information ?