Technical FAQs

Ask a Question

How to print alarms from the Web Applications/Alarms on a schedule basis?

Issue:
How to print alarms from the Web Applications/Alarms on a schedule basis?

Product Line:
Power Monitoring Expert Web Applications/Alarms

Environment:
 PME Web Applications

Cause:
Unable to print the alarms from Web Applications/Alarms on a schedule basis.

Resolution:
To print the alarms/Events from the Web Applications/Alarms, take the following steps
1. Select the Reports Tab from the Web Applications
2 Expand the General Folder under the Report Library and select the Event History Report
3. Select the options needed, generate the report and save it as shown on the screen shot below.


4. Subscribe the report, select the Format, Delivery Mode, Schedule needed  and save it as shown below.
Was this helpful?
What can we do to improve the information ?