Technical FAQs

Ask a Question

Preventa XCS - EC/EU declaration of conformity for the XCSZ01 ... XCSZ05 operating keys

We do not provide any EC/EU declaration of conformity for the XCSZ01 or XCSZ02 or XCSZ03 or XCSZ05 operating key sold separately, because the key is combined to some XCS safety switch. For the XCS safety switches, the EC/EU declaration of conformity concerns the couple XCS* + XCSZ*. Attached the EC/EU manufacturer declaration of the XCS series, dated on 2016. Note that the XCSZ* operating keys are not CE marked on the delivery plastic bag label.
Was this helpful?
What can we do to improve the information ?