Browse FAQs

Is it possible to operate Lexium 32 from DC bus only?

Published date: 04 September 2019

Yes, it is permitted to power and operate Lexium 32 directly from the DC bus only.

See attached presentation.

Note: You will need expert mode access in SoMove to modify the parameter for monitoring of missing mains phase.  The password for expert mode is 696969


rev 9-4-19

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.