Technical FAQs

Ask a Question

The EasyPact EZB fishbone type busbar can be extended for a bigger number of outgoers?

The EasyPact EZB busbars have the following extension possibilities:
- EZB250 - No extension possible;
- EZB400 - 1 piece of EZBNS2  OR  1 piece of EZBNS4;
- EZB630 - 1 piece of EZBNS2  OR  1 piece of EZBNS4.
Was this helpful?
What can we do to improve the information ?