Technical FAQs

Ask a Question

Osisense XC - Difference between the standard XCKT2510P16 limit switch and the adapted XCKT2510P16S27 switch

The difference between XCKT2510P16 limit switch and the adapted XCKT2510P16S27, is the head itself. The XCKT2510P16S27 uses a special rounded plunger head, not sold separately. The standard XCKT2510P16 uses the ZCE10 head. See attached picture showing both plunger heads. XCKT2510P16 data sheet @ http://www.tesensors.com/datasheet/XCKT2510P16/
The adapted XCKT2510P16S27 limit switch is available to order in 2017 without any marketing restriction.

Was this helpful?
What can we do to improve the information ?