Technical FAQs

Ask a Question

Does Schneider Electric offer a direct replacement for Berger Lahr motor type IFE71/2CAN-DS/-QBB54/2-064KSP54 with ID number of 66307190016

No, the Berger Lahr motor type IFE71/2CAN-DS/-QBB54/2-064KSP54 with ID number of 66307190016 is a special version for Atlas Converting in Europe
There ares some design features incorpoprated in this model which are unique to the OEM Atlas Converting.
This model uses a 64:1 gearbox which is not a standard ratio that offered in the catalog.
You must contact the OEM machine builder Atlas Conveting for spares or replacement.

rev 7.19.17
Was this helpful?
What can we do to improve the information ?