Technical FAQs

Ask a Question

What are SoMachine license updates (from version V3.0 or V3.1 to version V4.0 or later)

The SoMachine license updates (from version V3.0 or V3.1 to version V4.0 or later) are:

- SoMachine reference (V3.0/V3.1): MSDCHNLMUA (Single)
- Reference for update to SoMachine V4.3: SOMNADCZXSPAZZ (Single license)

- SoMachine reference (V3.0/V3.1): MSDCHNLMTA (Team)
- Reference for update to SoMachine V4.3: SOMNADCZXTPAZZ (Team license)

- SoMachine reference (V3.0/V3.1): MSDCHNLMFA (Facility)
- Reference for update to SoMachine V4.3: SOMNADCZXEPAZZ (Entity license)

Controllers for the solution (S-type controllers)
- SoMachine reference (V3.0/V3.1): MSDCHLLMUV3*S0, MSDCHLLMTV3*S0
- Reference for update to SoMachine V4.3: SOMNSDCZXTPAZZ
Was this helpful?
What can we do to improve the information ?