Technical FAQs

Ask a Question

Is the LV432520 safety trip interlock compatible with both Compact NS630 and Compact NSX630?

The safety trip interlocks for Compact NS630 and Compact NSX630 are not interchangeable.
The LV432520 is compatible only with Compact NSX range circuit breakers.
The safety trip interlock for the obsolete Compact NS630 circuit breakers has the reference number 32520.
Was this helpful?
What can we do to improve the information ?