Technical FAQs

Ask a Question

Unable to Load Framework error when opening web application

The following error message appears when opening PME web application:

          Unable to load framework
          There was a problem loading the Configuration Applications.

Product Line 
Power Monitoring Expert, PME (any version)

Web Application

Both conditions below contributed to the problem:

1. FlexNet Licensing Service was 'disabled' first, and then
2. Server was rebooted

Change the 'Startup type' of FlexNet Licensing Service to 'Automatic' and start the service.
Was this helpful?
What can we do to improve the information ?