Technical FAQs

Ask a Question

What are the operation function codes that are supported by M580 platform using MBP_MSTR function block?

The MBP_MSTR block is supported on various platforms like Momentum, Quantum and M580.
 
But only the following operation codes are supported on all M580 (Standalone/Hot Standby) platform CPUs:
 
 1 = Write data,
 2 = Read data,
14 = CIP Explicit Message
15 = Send Modbus Request
 23 = Read / Write data
 
Was this helpful?
What can we do to improve the information ?