Technical FAQs

Ask a Question

Osisense XC - 3D CAD file of the ZCE1A metal end plunger head with silicone boot

In the Traceparts library, the ZCE1A metal end plunger head with silicone boot does not exist. Please use the existing ZCE11 metal end plunger head with nitrile boot, at following Telemecanique Sensors web site @
http://www.tracepartsonline.net/(S(gq2sz4a550vu1i0ne4rx3xyf))/PartDetails.aspx?Class=TELEMECANIQUE_SENSORS&clsid=/F_TELEMECANIQUE_SENSORS/TELEMECANIQUE_SENSORS.010/TELEMECANIQUE_SENSORS.010.010/TELEMECANIQUE_SENSORS.010.010.020/TELEMECANIQUE_SENSORS.010.010.020.040/&ManID=TELEMECANIQUE_SENSORS&PartFamilyID=10-17052013-101257&PartID=10-17052013-101257&SrchRsltType=0&SrchRsltId=3
Difference between both end plunger head is the boot material, having no impact on the product dimensions
Was this helpful?
What can we do to improve the information ?