Technical FAQs

Ask a Question

Osisense XC - 3D CAD file of the ZCEA6 cat's whisker head

In the Traceparts library, the ZCEA6 cat's whisker head with silicone boot does not exist. Please use the existing ZCE06 cat's whisker head with nitrile boot, at following Telemecanique Sensors web site @
http://www.tracepartsonline.net/(S(gq2sz4a550vu1i0ne4rx3xyf))/PartDetails.aspx?Class=TELEMECANIQUE_SENSORS&clsid=/F_TELEMECANIQUE_SENSORS/TELEMECANIQUE_SENSORS.010/TELEMECANIQUE_SENSORS.010.010/TELEMECANIQUE_SENSORS.010.010.020/TELEMECANIQUE_SENSORS.010.010.020.040/&ManID=TELEMECANIQUE_SENSORS&PartFamilyID=10-17052013-097487&PartID=10-17052013-097487&SrchRsltType=0&SrchRsltId=3
Difference between both cat's whisker heads is the boot material, having no impact on the product dimensions
Was this helpful?
What can we do to improve the information ?