Technical FAQs

Ask a Question

Osisense XC - 3D CAD file of the ZCEA8 spring rod head

In the Traceparts library, the ZCEA8 spring rod head with silicone boot does not exist. Please use the existing ZCE08 spring rod head with nitrile boot, at following Telemecanique Sensors web site @
http://www.tracepartsonline.net/(S(ug1opwsx3uagiapa3jzqmfqc))/PartDetails.aspx?Class=TELEMECANIQUE_SENSORS&clsid=/F_TELEMECANIQUE_SENSORS/TELEMECANIQUE_SENSORS.010/TELEMECANIQUE_SENSORS.010.010/TELEMECANIQUE_SENSORS.010.010.020/TELEMECANIQUE_SENSORS.010.010.020.040/&ManID=TELEMECANIQUE_SENSORS&PartFamilyID=10-17052013-099057&PartID=10-17052013-099057&SrchRsltType=0&SrchRsltId=4
Difference between both spring rod heads is the boot material, having no impact on the product dimensions
Was this helpful?
What can we do to improve the information ?